Overview This guide explains how to configure Illustra Edge Analytics, specifically AI Object Classification and integrate it with ExacqVision Client. Following these steps allows you to view live analytics, search for specific objects (such as cars or people), and link analytics events within exacqVision. The same workflow can be applied to other analytics such as… Continue reading How to Configure Illustra Edge Analytics with exacqVision
Tag: camera configuration
Connecting an Illustra Camera to Two Servers Simultaneously
Description This article outlines the available methods for connecting a single Illustra camera to two servers at the same time. This is useful for environments where two recording or monitoring systems need simultaneous access to the same camera feed. Product Illustra IP Cameras exacqVision Server Solution Option 1 — Recommended Method (Official) Option 2 —… Continue reading Connecting an Illustra Camera to Two Servers Simultaneously
Samsung PNM-C34404RQPZ Use Hanwha Vision Plugin for connecting
Introduction We have seen issues with The Quality Control slider being greyed out under the camera settings when using ONVIF plugin. The Samsung PNM-C34404PQPZ Camera Device type should be using the Hanwha Vision Plugin. If these are using Onvif currently you can convert them to Hanwah Vision Plugin under the Add IP Camera section. Select… Continue reading Samsung PNM-C34404RQPZ Use Hanwha Vision Plugin for connecting
Unable to Update Camera Name Illustra 12MP Fisheye in Cloudvue or Cloudvue Manager
Warning: Level 2 Document – Please do not distribute. Description The Illustra 12MP Fisheye IPS12F27OIA4 camera name cannot be changed in either Cloudvue or Cloudvue Manager.An error is displayed when attempting to save the updated camera name. Product Steps to Reproduce Expected Results The camera name should update successfully and reflect the new name… Continue reading Unable to Update Camera Name Illustra 12MP Fisheye in Cloudvue or Cloudvue Manager