Connecting an Illustra Camera to Two Servers Simultaneously

Description This article outlines the available methods for connecting a single Illustra camera to two servers at the same time. This is useful for environments where two recording or monitoring systems need simultaneous access to the same camera feed. Product Illustra IP Cameras exacqVision Server Solution Option 1 — Recommended Method (Official) Option 2 —… Continue reading Connecting an Illustra Camera to Two Servers Simultaneously