Introduction OAuth authentication can succeed for multiple exacqVision components while still failing for Enterprise Manager synchronization in exacqVision Client version 26.0.2.0 when using MS Entra ID. Problem The exacqVision Client reports that OAuth is not configured on the Enterprise Manager server when attempting to synchronize systems. Cause The failure occurs specifically during the Client-to-Enterprise Manager… Continue reading OAuth Login Succeeds but Enterprise Manager Sync Fails using Entra IDP