Introduction OAuth authentication can succeed for multiple exacqVision components while still failing for Enterprise Manager synchronization in exacqVision Client version 26.0.2.0 when using MS Entra ID. Problem The exacqVision Client reports that OAuth is not configured on the Enterprise Manager server when attempting to synchronize systems. Cause The failure occurs specifically during the Client-to-Enterprise Manager… Continue reading OAuth Login Succeeds but Enterprise Manager Sync Fails using Entra IDP
Tag: server-side Oauth
OAuth – Microsoft Entra App Registration Requirements for exacqVision version 26
Introduction Starting with exacqVision version 26, Enterprise Manager and ExacqVision Client & Server support OAuth authentication using Microsoft Entra ID for access to Enterprise Manager (EM), and the exacqVision Client NVR access. Proper configuration of redirect URIs within Microsoft Entra is required for OAuth authentication to succeed. Problem OAuth authentication may fail with redirect URI… Continue reading OAuth – Microsoft Entra App Registration Requirements for exacqVision version 26