Description: Certain Axis camera models configured with 4K resolutions (2840×2160 or higher) do not display the selected resolution in the Resolution drop-down menu within the Exacq client on Linux systems. Although the resolution field appears blank in the user interface, the camera continues to operate and record correctly at the configured 4K resolution.This issue occurs… Continue reading Linux 4 K Camera Resolution Drop Down Menu Not Displaying Resolution