The Django CSRF_TRUSTED_ORIGINS setting provides a mechanism for configuring a list of trusted origins for unsafe HTTP requests for Linux Enterprise Manager host servers. The list is empty by default. This is configured by setting up a Linux SYSTEM Environment variable. When configured, Enterprise Manager will initialize the configured list on startup. This may be… Continue reading Configuring Django CSRF_TRUSTED_ORIGINS for use with Enterprise Manager – Linux
Tag: CSRF
Configuring Django CSRF_TRUSTED_ORIGINS for use with Enterprise Manager – Windows
The Django CSRF_TRUSTED_ORIGINS setting provides a mechanism for configuring a list of trusted origins for unsafe HTTP requests for Windows Enterprise Manager server hosts. The list is empty by default. This is configured by setting up a Windows or Linux SYSTEM Environment variable. When configured, Enterprise Manager will initialize the configured list on startup. In… Continue reading Configuring Django CSRF_TRUSTED_ORIGINS for use with Enterprise Manager – Windows
Product Security Advisory: exacqVision Vulnerability impacting exacqVision Web Service (CSRF)
Disabling the CSRF on Enterprise Manager 24.12 and higher
In some cases, CSRF would prevent accessing the EM server from the browser due to the CSRF “Cross-Site Request Forgery” validation when having a proxy server, and needs to disable this protection. Product Enterprise Manager version 24.12 and higher Steps to Disable -Windows -Linux