Axis Body Worn Hard Cap User of 128

Description:  In Exacq Server version 26.0.2.0 and previous versions, the Axis Body Worn integration is limited to a maximum of 128 Body Worn Users. When a 129th user is added, the Axis W800 System Controller will generate an error indicating that the user limit has been exceeded.  Administrators can confirm this by logging into the Axis… Continue reading Axis Body Worn Hard Cap User of 128

Axis Body Worn Camera / User Transfer

Warning: Level 2 Document – Please do not distribute.   Description Can Users and Cameras be transferred from one Exacq Server to another? Product Axis Body Worn Cameras. The answer is no.It would be a new server, so the body worn system would need to be decommissioned and then reconfigured into the new system. Add… Continue reading Axis Body Worn Camera / User Transfer