Fresh Install Enterprise Manager 24.12 on Linux

Product  Requirements Ubuntu 20.04 or higher Manually installing PostgreSQL 17 Remove any installed EM server if existed Installing PostgreSQL Update Ubuntu repository list sudo apt-get updatesudo apt-get upgrade Install PostgreSQL 17 Note: Ensure that the line is `local all postgres trust`. Sometimes you would need to allow access via TCP/IP in the pg_hba.conf file Creating… Continue reading Fresh Install Enterprise Manager 24.12 on Linux

Motion is not working for All ONVIF cameras on Exacq Server 24.06 & 24.09

Description Motion recording is not working on all ONVIF cameras with Exacq server version 24.06 & 24.09. Some analytics may not work on some brands. Product  Exacq server versions 24.06 & 24.09 Steps to Reproduce  Connecting ONVIF cameras or any supported brands via ONVIF to exacq server ver 24.06 or 24.09 and trying to trigger… Continue reading Motion is not working for All ONVIF cameras on Exacq Server 24.06 & 24.09

Ccure 9000 Door Held Event issue with Exacq 24.06 and earlier

Description When Activating an event for the door held on Ccure, it will not get activated on Exacq side and will not get triggered via event linking. Product  Exacq Server and Client versions 24.03 & 24.06 Ccure 9000 & Firmware=”web=7.0.1174.174, app=4.0.0″ Steps to Reproduce Creating the door held event on Ccure side then trying to… Continue reading Ccure 9000 Door Held Event issue with Exacq 24.06 and earlier

Performance issue when analytics enabled on Exacq

Description  issues with analytics enabled where-as the server will eventually become unresponsive and reboot after a short time. Product ExacqVision Server versions 23.09 & 24.03 & 24.06 Steps to Reproduce  1) install 23.09.9.0 exacqvision server software2) connect illustra Pro4 20mp IPS20-M12-OIA4 using firmware SS017.06.05.00.0083) Verify analytics are enabled on the cameras – analyticmetadata, objectdetection, motiondetection4)… Continue reading Performance issue when analytics enabled on Exacq

De-elevation not working on Ubuntu 20.04 and higher

Product  exacqVision Server Steps to reproduce Use the following command per the hardening guide sudo dpkg-reconfigure –p low edvrserver Expected Results  De-elevating the exacqVision Server Actual Results  Getting the following error Solution The fix for this issue will be back patched to 24.03.X We strongly recommend checking our Exacq server release notes to be aware… Continue reading De-elevation not working on Ubuntu 20.04 and higher

Kantech – Entrapass ver 8.70 & 8.62 stops showing the outputs and inputs in exacqVision

Description When connecting exacqVision Server to Entrapass versions 8.62 & 8.70 or updating Entrapass to these versions, it will stop showing the inputs in exacqVision. Product exacqVision Server any version with Kantech Entrapass ver 8.62 & ver 8.70. Steps to Reproduce Expected Results All Kantech inputs are displayed. Actual Results Solution The Kantech team has… Continue reading Kantech – Entrapass ver 8.70 & 8.62 stops showing the outputs and inputs in exacqVision

Analytics Email attachment is causing a High CPU utilization

Description When setting Event Linking for analytics to attach a video to the email notification, it would cause a high CPU utilization Product exacqVision Server 23.09.6.1 Steps to Reproduce Expected Results Send emails with attachments without any issues. Actual Results Not sending all the emails and causing a high CPU utilization and may crash the… Continue reading Analytics Email attachment is causing a High CPU utilization

Can’t reinstall the EM server

When uninstalling Exacq EM server version 23.06 or above and reinstalling it again on the Windows unit, It will not complete the installation and ask to close the open session even if no sessions are open. Root cause The root cause of this issue is The Microsoft Open Database Connectivity (ODBC) that was not removed… Continue reading Can’t reinstall the EM server

Can’t Set an Email Profile When Kantech Software is Connected to The Exacq Server

Description When having Kantech Board connected to the Exacq Server, Client Software keeps refreshing the configs and that prevents the Exacq client from creating an Email notifications profile. affected version is 23.03 or lower Solution Updating ExacqVision Server and Client to version 24.03 or above. Updating the Kantech Entrapass to version 8.80 or above.

LDAP connection requirements

Description:- In order to succeed in the remote client authentication via LDAP, We will need to make sure that we have the following three points. The way Kerberos tickets work is that we need all three points able to see and connect to each other, so we need to check these requirements before establishing the… Continue reading LDAP connection requirements