Categories
exacqVision Server Windows Knowledge Support Support exacqVision Server Categories Products

Kantech – Entrapass ver 8.70 & 8.62 stops showing the outputs and inputs in exacqVision

Description

When connecting exacqVision Server to Entrapass versions 8.62 & 8.70 or updating Entrapass to these versions, it will stop showing the inputs in exacqVision.

Product

exacqVision Server any version with Kantech Entrapass ver 8.62 & ver 8.70.

Steps to Reproduce

  1. Connect the exacqVision server to Kantech version 8.70 or 8.62.

Expected Results

All Kantech inputs are displayed.

Actual Results

  • Kantech inputs do not appear
  • Connections drop leading to loss of inputs within exacqVision.

Solution

The Kantech team has provided a solution with the following steps.

  1. Stop Smartlink
  2. As a precaution, make a backup copy of the following directory:
    C:\Program Files (x86)\Kantech\Smartlink_CE
  3. Copy the following 2 executables to C:\Program Files (x86)\Kantech\Smartlink_CE\Bin

    EpCeSmartLink.exe
    EpCeSmartlinkService.exe

  4. Start Smartlink