Description
The Axis cameras are choppy and freezing on the exacqVision Client Live view page and when checking the logs showing.
AxisPI Warning 10.100.1.35 EdgeStor - error 56 attempting to get<br>the list of disks. This command will be retried in 30 seconds..
AxisPI Verbose 10.100.1.35 Network error 56 from request<br>axis-cgi/disks/list.cgi?diskid=all using scheme https.
Product
exacqVision Server 22.03 to 22.06
Steps to Reproduce
Install exacqVision Server version 22.03 or 22.06 and connect to Axis cameras
Solution
Updating the ExacqVision server to version 22.09.5.0
Windows 64bit, here
Windows 32bit, here
Ubuntu Linux 64bit, here
Ubuntu Linux 32bit, here