LDAP connection requirements

Description:-

In order to succeed in the remote client authentication via LDAP, We will need to make sure that we have the following three points.

  • ExacqVision Server uses an enterprise license and is connected to an AD/LDAP server.
  • ExacqVison Client is able to reach the Exacq Server via port 22609, and the LDAP via port 636 if LDAP with SSL or 389 if LDAP without SSL.
  • Active Directory server can reach the Exacq Server and Exacq Client workstation.

The way Kerberos tickets work is that we need all three points able to see and connect to each other, so we need to check these requirements before establishing the Exacq client connection to the Exacq server via the SSO method.