Axis Motion Recording on PTZ Movement

To enable motion based recording on an Axis device during PTZ movement, complete the following steps: <br>

On the Axis camera’s web page, configure a recipient for the event. The Type should be TCP; the IP address should be the address of the exacqVision server; the port can be any open port. <br>

Configure the rule on the Axis camera’s web page. Trigger should be PTZ and Moving; Schedule should be Always; Type should be Send Notification; Recipient should be the recipient from the previous step; the message should be the keyword that exacqVision is listening for to trigger the event. Note the message for later. This example uses the last two digits of the IP address and the input number on the encoder. Select the option to send notifications continuously while the trigger is active. <br>

In exacqVision Client, select Serial Profiles. Enter a name and click Apply. Click New under Event Keywords and enter the message created in the previous step. Click Apply again. <br>

In exacqVision Client, select Serial Ports. Click New. Use should be Access Ctrl; the name can be any identifier; Type should be TCP Listener; Address should be the IP address of the Axis device; Port should be the port assigned in step 2; timeout should be 0 (zero). <br>

In exacqVision Client, select Event Linking. Click New. Event Type should be Serial Port; Event Source should be the serial profile that includes the key word message; Action Type should be Record Video; Action Target should be the device that we want to record motion on PTZ movement; Post-Trigger should be at least five seconds to ensure that the correct amount of data is recorded after the command has been issued. <br>