Remote Updates Fail on Windows-based exacqVision Servers

On some Windows-based exacqVision servers with exacqVision software earlier than version 5.8, remote updates can fail if the system time changed between the time the system was started and the time the remote update is initiated. <br> To work around this issue, stop and restart the exacqVision Server service, and then immediately initiate the remote… Continue reading Remote Updates Fail on Windows-based exacqVision Servers