Cannot clear a “Power Supply” alarm with USB DIO module attached

The alarm is being generated by the USB DIO module attached to the system. To remove: Windows If logged in as the OS user, close the exacqVision Client by pressing Alt+F4.Log out of the user and into admin by selecting Start > Log Out > select admin > type admin256 > press Enter. Note: admin256 is default. If this… Continue reading Cannot clear a “Power Supply” alarm with USB DIO module attached

LED lights on USB DIO box

A USB DIO box contains red and green LED lights that indicate various conditions:<br> Solid red: system startupFlashing red: errorSolid green: actively communicating with server or other applicationFlashing green: driver loadedIf the green light does not stop flashing, the server is not communicating for some reason. Restart the server or the exacqVision Server service if this occurs.<br>