Introduction exacqVision can ingest serial data (for example POS/ATM/access-control text strings) and then use Serial Profiles to store, display, search, and trigger actions from that data. Serial data is typically unencrypted, clear-text/ASCII characters delivered either through a physical serial interface (UART/RS-232/RS-485) or over the network (serial-over-IP). This article explains how the Serial Port “Type” options… Continue reading Difference Between TCP, TCP Listening, HTTP, and UDP Serial Profile Protocols in exacqVision