Description Steps to create a desktop shortcut launcher for the exacqVision Client for either Ubuntu 18.04 or 20.04 Product exacqVision Client Solution <br>
Tag: Shortcuts
Opening exacqVision Client on Separate Monitors Using Short Cuts with Client 9.4 and Higher
In some installations users may want to allow users to automate the process of opening multiple client instances on different monitors of a workstation. This article details the steps to create an XDV file that will open the client to the configuration of your choice. Click the exacqVision logo in the top-right corner of the client… Continue reading Opening exacqVision Client on Separate Monitors Using Short Cuts with Client 9.4 and Higher
exacqVision Client Keyboard Shortcuts
Keyboard ShortcutFunctionAvailable In…F1View context-sensitive online HelpAll exacqVision Client pagesF3Display Find Camera windowLive pageF4Hide/show navigation panelAll exacqVision Client pagesF8Hide/show message bar, date/time bar, and toolbarAll exacqVision Client pagesF11View exacqVision Client in fullscreen modeAll exacqVision Client pagesAlt+EnterCombines F4, F8, and F11 functionalityAll exacqVision Client pagesPage UpZoom in (analog or digital PTZ)Live pagePage DownZoom out (analog or digital… Continue reading exacqVision Client Keyboard Shortcuts