Associations Not Allowed to be saved as Momentary or Sustained Option

Description  When setting up a new association there is no options in the drop down menu for Momentary or Sustained when setting up Associations. Display only is seen as the only option available. This was exhibited on Server/ Client software starting on 23.09 through 24.12.7. Product  Steps to Reproduce  Upon update from 23.06 Server/Client to… Continue reading Associations Not Allowed to be saved as Momentary or Sustained Option

Enterprise Manager Server Configuration Backup

Saving backups of your ExacqVision server configurations is important in maintaining your system environment, or getting a system back up and running quickly if needed. Learn to automate saving regular backups, or manually save configurations, using Enterprise Manager.