Creating a Self-Signed SSL Certificate

Before Beginning… Requirements You will need the OpenSSL program to create a self-signed certificate. The method of obtaining this program varies based on the operating system used. Note: A certificate generated on either platform will work on the other (i.e.- a certificate generated using openssl on Linux can be used with a Windows web service).… Continue reading Creating a Self-Signed SSL Certificate

Self-signed and Untrusted Private/Internal Certificates Cannot be Validated in the ExacqVision Client

Description  ExacqVision Client software is unable to validate Self-signed and untrusted private or internal certificates Product  Steps to Reproduce  Expected Results  Actual Results  Solution

Enabling HTTPS For exacqVision Enterprise Manager Versions 22.06 thru 24.09

For Instructions on exacqVision Enterprise Manager version 22.03 or older see Knowledge Base Article #12724 The following document details how to enable HTTPS connections to exacqVision Enterprise System Manager from update 22.06 thru 24.09.2.1. For a trusted certificate, it is recommended that you purchase a third-party intermediate certificate from one of many online providers. If… Continue reading Enabling HTTPS For exacqVision Enterprise Manager Versions 22.06 thru 24.09

Enabling HTTPS For exacqVision Enterprise Manager Versions 22.03 or Lower

IMPORTANT For Instructions on current versions of exacqVision Enterprise Manager versions 22.06 or higher see Knowledge Base Article #12804 This document details how to enable HTTPS connections to exacqVision Enterprise System Manager on versions 22.03 or lower. For a trusted certificate, it is recommended that you purchase a third-party intermediate certificate from one of many… Continue reading Enabling HTTPS For exacqVision Enterprise Manager Versions 22.03 or Lower

ESM May Not Connect to Web Service with Self-Signed Certificate

Symptom: The camera video feed section in ESM displays an SSL error message. <br> Problem: ESM may not connect to the exacqVision Web Service if the web service is using a self-signed certificate. This may be more prevalent on systems where TLS/SSL was configured after being added to ESM. ESM did not automatically detect the… Continue reading ESM May Not Connect to Web Service with Self-Signed Certificate

Camera-to-Recorder HTTPS Connections

exacqVision supports connecting to many cameras using HTTPS. Depending on the camera firmware capabilities and the device type plugin used in exacqVision the level of encryption provided may vary. Using the IP Camera Integration Database, you may choose to filter the displayed results by devices which support SSL (HTTPS). <br> Connecting with HTTPS When adding… Continue reading Camera-to-Recorder HTTPS Connections