Description Hanwha will not allow motion to work properly with Exacq Server 24.09.4.0 as long as the camera is on fw 23.01.04-20240417-R929 due to a NTP issue found. Another issue reported is the connection status will throw errors to indicate it is not connected properly.NOTE:FW 23.01.01 obtained from Hanwha (which will be the official release… Continue reading Hanwha PNM-C32083RVQ Connection to Server and Motion Stops Working
Tag: Samsung Motion
Samsung Motion Issues
Description Samsung cameras have experienced motion recording issues when running exacqVision Server version 22.09 or lower. Product Steps to Reproduce Expected Results Actual Results Solution It was determined this was a result of metadata timeouts and can be resolved by updating to exacqVision Server 22.12.3.0 or higher.