ExacqVision Server version 9.8 or higher requires Windows PowerShell.

Symptom: exacqVision Server service fails to start with Error 1053:  The service did not respond in a timely fashion.   <br> Problem: Windows Server 2008 does not include Windows PowerShell which is required on exacqVision Server versions 9.8 or higher. <br> Solution: Option 1:  Stay at exacqVision Server 9.4 Option 2: Upgrade the operating system to a supported… Continue reading ExacqVision Server version 9.8 or higher requires Windows PowerShell.