Replacing a Drive in an LSI 3ware RAID Array

To install a replacement drive in an exacqVision system with an LSI 3ware RAID array, complete the following steps.<br> NOTE: This procedure requires a Phillips-head screwdriver and approximately 20 minutes to complete.<br> If applicable, close the exacqVision Client software, log out of the operating system user account, and log in as an administrator. To log out… Continue reading Replacing a Drive in an LSI 3ware RAID Array

SMART Attributes May Not Appear for LSI RAID Disks

Symptom: S.M.A.R.T. attributes do not appear for hard disks attached to the LSI RAID controller.  <br> Problem: Issue introduced with exacqVision Server 9.2.3 when support was added for the F2A chassis model using the LSI HBA. <br> Solution: Update exacqVision Server version to 9.4.0 or higher.   <br>