ONVIF PTZ camera with two streams may display as two different cameras even if “Manage all streams as quality” is checked

Product exacqVision Server 6.2 to 7.2.3 <br> Symptom ONVIF PTZ camera with two streams may display as two different cameras even if “Manage all streams as quality” is checked. This is because the XML is reporting the secondary context as being an independent PTZ which is something generally used for fisheyes where PTZing one stream… Continue reading ONVIF PTZ camera with two streams may display as two different cameras even if “Manage all streams as quality” is checked

Multistreaming and Auto-Context Switching

Multistreaming Multistreaming provides the ability to display or record camera video streams at alternative settings for a number of different use cases. Examples include: NOTE: Multistreaming is not available for exacqVision Start users and your cameras must support multistreaming. Refer to the IP Camera Integration database to search for supported camera models. <br> Adding Streams… Continue reading Multistreaming and Auto-Context Switching