Description Cameras are not able to switch to Serial IP under Mechanical tab.Looking at the Onvif plugin the PTZ for the camera was set to “0”We could not enable it in the client. When attempting to set the serial to IP in the mechanical PTZ tab, it would flip back to the Serial Port to… Continue reading Allibi Camera ALI-PZ40-UZAI PTZ is disabled by default on 23.06-24.03
Tag: PTZ Camera
ONVIF PTZ camera with two streams may display as two different cameras even if “Manage all streams as quality” is checked
Product exacqVision Server 6.2 to 7.2.3 <br> Symptom ONVIF PTZ camera with two streams may display as two different cameras even if “Manage all streams as quality” is checked. This is because the XML is reporting the secondary context as being an independent PTZ which is something generally used for fisheyes where PTZing one stream… Continue reading ONVIF PTZ camera with two streams may display as two different cameras even if “Manage all streams as quality” is checked