Description Cameras are not able to switch to Serial IP under Mechanical tab.Looking at the Onvif plugin the PTZ for the camera was set to “0”We could not enable it in the client. When attempting to set the serial to IP in the mechanical PTZ tab, it would flip back to the Serial Port to… Continue reading Allibi Camera ALI-PZ40-UZAI PTZ is disabled by default on 23.06-24.03
Tag: PTZ
Motion Event PTZ Presets with the Axis M5000-G in exacqVision
Overview The Axis M5000-G PTZ camera is a multi-sensor camera containing three stationary wide-angle lenses around the circumference of the camera body and one center-mounted PTZ lens. This guide is intended to help users automate the positioning of the PTZ lens upon events, such as motion detection. Requirements NOTE: While this article is written specifically… Continue reading Motion Event PTZ Presets with the Axis M5000-G in exacqVision
Samsung QNP-6230x Motion not Working After Selecting a PTZ Preset
Description After selecting a PTZ preset motion appears to stop working in the camera’s web interface. If you edit the motion settings in the client, the motion will events will start to work in the camera again. Product Camera models: Firmware: Steps to Reproduce Have the camera setting on the home preset. Expected Results PTZ… Continue reading Samsung QNP-6230x Motion not Working After Selecting a PTZ Preset
Maps Item Icons Incorrect
Description Customer would like to change some map icon graphics, some bullet cameras are displayed as domes on the map graphic. He has asked if there is a config file that contains the map graphic information Product Steps to Reproduce Expected Results Expected box camera Icon Actual Results PTZ/Dome camera Icon Solution This is expected… Continue reading Maps Item Icons Incorrect
Using the ADVCPTZKEY1 USB Joystick / Keyboard with exacqVision
This document will guide you through step-by-step procedures for keyboard use and suggested button mappings. Prerequisites For proper operation of the American Dynamics ADVCPTZKEY1 PTZ USB Keyboard, both the exacqVision Client and Server must be on version 22.03 or higher. Product ADVCPTZKEY1 American Dynamics Surveillance Keyboard <br> Setup <br>
USBDIO Modules connected to IP only NVRs will not have the PTZ use option
This is because that control should be provided by the encoder and the PTZ plugin is not installed. <br>
Mechanical PTZ tab will not show up for Samsung cameras
When updating ExacqVision Server straight to 21.03 from a version prior to 9.8 the mechanical PTZ tab disappears. On the previous version below 9.8, update to ExacqVision Server 19.12 and verify the mechanical PTZ tab is there. Then update to ExacqVision Server 21.03 and verify the mechanical PTZ tab is there. If it is not,… Continue reading Mechanical PTZ tab will not show up for Samsung cameras
Does Exacq use the Bosch BiPhase PTZ Protocol
No, Exacq uses the Bosch OSRD Protocol. To send BiPhase you will need a converter like the LTC8786, which connects to the DB9 RS232 port on the back of the unit.
ONVIF PTZ camera with two streams may display as two different cameras even if “Manage all streams as quality” is checked
Product exacqVision Server 6.2 to 7.2.3 <br> Symptom ONVIF PTZ camera with two streams may display as two different cameras even if “Manage all streams as quality” is checked. This is because the XML is reporting the secondary context as being an independent PTZ which is something generally used for fisheyes where PTZing one stream… Continue reading ONVIF PTZ camera with two streams may display as two different cameras even if “Manage all streams as quality” is checked
Saved Digital PTZ View displays incorrectly when searching
Product exacqVision Client 6.0 to current <br> Description If you use the same video input, one with digital PTZ enable and zoomed in and the other with Digital PTZ disabled, the saved view will not display as intended when searching that view on the Search Cameras page. <br> Solution Enable Digital PTZ on both instances.… Continue reading Saved Digital PTZ View displays incorrectly when searching