Description If the exacqVision Server data drives are full and are displaying “Recording Not Possible” on the storage page then it is possible an invalid hour folder was created during the switch to Daylight Savings Times (DST). Use the following instructions to verify and resolve the issue. Product Solution These instruction are based on Windows… Continue reading Recording Not Possible – Windows DST Issue
Tag: psfpi
False Drive Offline status on some Q-series models
Description Some drives may show an “offline” status on the hardware tab in ExacqVision Client when Server Version 23.03.1.0 is installed on Q-series models, though data can be read from and written to the drive.Note: This issue manifests itself cosmetically by appearing as if the drive is offline but has no bearing on functionality for… Continue reading False Drive Offline status on some Q-series models