When troubleshooting TCP/IP connectivity issues, it is often helpful to confirm that the network path is open over a specified port and that there is no interference from a firewall or antivirus. This also rules out software level problems that may be causing a failure to connect. While there exists many utilities to accomplish this… Continue reading PortCheck Utility
Tag: Port
The camera is showing connected but not streaming videos
If the camera is connected to ExacqVision Server and showing connected on the add IP camera page but not streaming videos and showing acquiring video. That means the RTSP streaming port may need to be opened on the Firewall, normally 554
ESM needs to use port and address when building xdv for client
Description If multiple servers share the same IP but have different ports. ESM will remove additional servers with same IP, only using one of the servers. It should include all of these servers. <br> Tested version 4.9.23 <br> Platform All <br> Steps to reproduce Add multiple servers on ESM with same IP Address and different… Continue reading ESM needs to use port and address when building xdv for client
exacqVision G-Series PoE Network Video Recorder
Can I change the default port for my ONVIF camera?
ExacqVision allows you to enter custom ports for cameras that have had standard port numbers changed. When selecting ‘ONVIF’ from the ‘Device Type’ selector in the process of adding a camera, the ‘Port’ field is greyed out. Rather than using the ‘Port’ field you will need to add the port number at the end of… Continue reading Can I change the default port for my ONVIF camera?
How do I change the listening port number for exacqVision Server?
By default, the exacqVision Client communicates with exacqVision Servers on port 22609. If your network does not allow port 22609, or if you need to forward the port on multiple exacqVision systems, you can change the exacqVision Server’s listening port number. To do this, complete steps detailed on this page. NOTE: The exacqVision Default Ports… Continue reading How do I change the listening port number for exacqVision Server?