Pelco SMLE1-15V5-3h Motion Events are not Received by Exacq

Description  The Pelco SMLE1-15V5-3h does will not record or see last motion events in exacq client/ server.Both Firmware’s were tested and work with the override.4.80.0.24(F722c136)and fw 4.86.0.20(7a7d6563) Product  ExacqVision Server 24.03.7.0 – 24.09.4.0 Steps to Reproduce  Set up motion in the cameras gui for each head in the camera to enable motion events. Expected Results … Continue reading Pelco SMLE1-15V5-3h Motion Events are not Received by Exacq

Enabling Multistreaming on Pelco Cameras

To enable mutlistreaming on compatible Pelco cameras, you must adjust settings in the camera’s web interface. Select the A/V Streams tab and ensure that both streams are configured for the H264 Compression Standard. NOTE: If the secondary stream is greyed out and not available for changes, adjust the primary stream settings until the secondary stream settings… Continue reading Enabling Multistreaming on Pelco Cameras