Description A NotifyPI enhancement was released with 8.4 which added the ability to specify ‘when’ to send an email: ‘Alarm Starts’, ‘Alarm Ends’ or ‘Alarm Starts and Ends’). However, the ‘Alarm Ends’ selection was failing to send the email when the trigger event (alarm) duration was shorter than the ‘Send Rate Limit’.If the event duration… Continue reading notifypi – failure to send email on falling edge
Tag: NotifyPI
NotifyPI fails with cURL error 55
Symptom: Email notifications fail to be received. <br> Problem: Server logs resemble: 15/12/2016 2:54:54 PM NotifyPI Warning Profile Description: Playground. Notification attempt return code= 55 15/12/2016 2:54:54 PM NotifyPI Verbose curl: (55) MAIL failed: 530 15/12/2016 2:54:54 PM NotifyPI Error Failed to send notification using profile Playground. This message will be retried This is caused… Continue reading NotifyPI fails with cURL error 55