Description Some Exacq NVRs built with Microsoft Windows Server 2022 only acknowledge one network interface, rather than two, when being configured out-of-box. <br> Product Issue has been noted on BBE systems ASRock Industrial IMB-X1313 system boards, listed below. NOTE: Windows Server OS is an optional upgrade for many systems, so this will not apply to… Continue reading Windows Server 2022 Showing Only One Network Card
Tag: NIC
Guidance on Using USB Network Interface Adapters
On occasion, Exacq Support is asked about using a USB network interface (NIC) on their system. This is more frequently asked by those with smaller units which may have only one network interface and a user is attempting to add additional network interfaces to span networks or attempt to increase network throughput by bonding/teaming multiple… Continue reading Guidance on Using USB Network Interface Adapters
Configuring IP Addresses on a Cloudvue Gateway
Description This article describes how to set IP addresses as either static or DHCP for a Cloudvue Gateways onboard NICs. Product Prerequisites Solutions NOTE: Network Settings can only be viewed, not changed from cloudvue.com Local Cloudvue Command Line In this example both NICs em2 (LAN) and em1 (Cameras) are being set to a static IP… Continue reading Configuring IP Addresses on a Cloudvue Gateway
NIC Bonding with Windows Server 2016 is only available through Server Manager
Description Servers with Windows 10 or Linux allow bonding to be configured via exacqVision Client. However, servers with Windows Server 2016 currently do not. Instead, bonding must be configured via Windows Server Manager: Product Expected Results Actual Results Solution <br>
Second on board NIC missing
Description There have been a couple of servers manufactured at the Bentel facility with Q87 motherboard that does not detect the second on board NIC out of the box. This is due to a bios misconfiguration during manufacturing. <br> Platform Linux and Windows with Q87 motherboard The servers we found in the field with this… Continue reading Second on board NIC missing
Example Network Diagram for Multi-NIC Systems
Best practice for servers with more than one NIC includes isolating camera traffic to a separate scheme. This practice not only isolates camera bandwidth consumption from other network traffic, but also adds an additional layer of security to prevent workstation users from accessing cameras and video streams directly. Whether using separate network switches or creating… Continue reading Example Network Diagram for Multi-NIC Systems
NIC Bonding on exacqVision Client and Server
Beginning with version 5.10, NIC bonding is supported on exacqVision Client and Server. The following sections contain requirements and steps for enabling NIC bonding. <br> Linux Ubuntu 10.04 and Later Install ifenslave-2.6 package. <br> apt-get install ifenslave-2.6 <br> Add bonding module to modules list by editing /etc/modules. <br> sudo gedit /etc/modules <br> Add “bonding” at… Continue reading NIC Bonding on exacqVision Client and Server
How is exacqVision NVR software licensed?
The exacqVision VMS software licenses a specific number of channels to a key based upon the server NIC’s MAC address. A license includes the maximum number of IP devices, an SSA period for software updates, analog video channels for Hybrid NVRs, and the functional level for the software. The functional levels are: See the Features… Continue reading How is exacqVision NVR software licensed?