Johnson Controls Updated NDAA 2019
Tag: NDAA
M-Series – Updating exacqVision Software
In order to comply with the NDAA “National Defense Authorization Act”, a two-step process is required to update an M-Series. First you must upgrade to version 20.03, then the server and webserver can be upgrade to the latest version. exacqVision Client versions higher than 20.03 are not supported. Note: The exacqVision Client version should not be… Continue reading M-Series – Updating exacqVision Software
Certain Illustra models may cause recording to stop
Description Certain models of Illustra cameras, on connection, may cause server to stop streaming from all other Illustra cameras. Steps to reproduce Add a ISL02P6OCWTT, firmware 0.0.0.15 (Local for Local camera that doesn’t comply with NDAA) Expected result all supported illustra3 cameras continue to record Actual result all illustra3 cameras stop recording (plugin’s read thread… Continue reading Certain Illustra models may cause recording to stop