When changing the windows for the HikVision cameras to the corridor mode, it will not trigger the motion on the bottom because it’s not supported by Exacq yet. This feature will be supported on the ExacqVision Server version 22.03.
Tag: Motion Not Supported
Samsung / Hanwha Cameras Show “Motion Not Supported”
Before being able to manage motion windows from the exacqVision Client the following actions need to be performed within the camera’s web GUI. You should now be able to manage existing areas and draw new areas from within the exacqVision Client Note: It may be necessary to factory reset the camera first. <br>
Troubleshooting Motion Not Supported
If you run in to an Exacq system where it says “Motion Not Supported” there are several camera manufacturers where you have to Enable Motion in the Web GUI of the device; as well as setting it in Exacq Client software. It will be listed under something like Analytics>Motion or Alarms or Motion.