Categories
Knowledge Support Support exacqVision Client exacqVision Server Categories Products

Motion Not Recorded

Are you seeing colored borders around the live video panels in the exacqVision Client when motion appears to be occurring?

<br>

Yes: Go to the Camera Time section below.
No: Go to the Motion Area section below.

NOTE: If the camera is configured to detect motion and also configured for Free Run recording on its schedule page, you will see the blue borders when motion occurs, but you will record ALL video even if motion is not occurring.

<br>

Camera Time

  1. Check the on-screen display (OSD) of the camera in Live view to verify the correct date and time (including AM/PM). To display the OSD, open the Configuration page, select the camera in the site tree, select the Display tab, and select the appropriate checkboxes.
    <br><br>
  1. If the time is inaccurate, go the camera’s configuration page. Ensure that the camera’s time zone is configured for GMT (-0).<br><br>
  2. On the exacqVision Add IP Cameras page, disconnect and reconnect the camera to try to sync the time.
    <br><br>
  1. If you continue to see an issue with recording motion video, verify the network time server’s IP. To do this, open the System page and select the Date/Time tab. Enter the local server’s IP address in the box and click Apply. Once again, deselect and reconnect the camera on the Add IP Cameras page.

    NOTE: Do not select Enable Override unless you want to sync the camera to a non-exacqVision NTP server, or if third-party software (such as anti-virus software or a firewall) blocks the exacqVision server from sending its address to the camera.
  1. Verify the camera’s firmware matches test records at https://exacq.com/support/ipcams.php. Upgrade if necessary.<br><br>
  2. Check the camera’s log files.

<br>

Motion Area

  1. Select the camera in the site tree to open its settings page.<br><br>
  2. Select the Motion tab. Then select either Motion Window or Motion Mask.<br><br>
  3. Determine which area is masked and in which area motion would be detected. (Some camera models allow more than one motion window.)<br><br>
  4. If necessary, increase Sensitivity or reduce the Percentage area. (Percentage is not available on some camera models.)<br><br>
    <br><br>
  5. If you still don’t see blue motion borders as expected, open the Client page and make sure the Show Record Status Border option is selected.
    <br><br>
  6. If you still don’t see blue motion borders as expected, open the Schedule tab on the camera’s settings page and make sure a recording schedule is configured.

<br>