Description The Panasonic WV-S8531N fails to detect motion when using H265 option. Product ExacqVision Server Steps to Reproduce Expected Results Motion is detected and video records. Actual Results Motion is not detected and video is not recorded. Solution Updating firmware to S8531_202ES allowed the camera use Motion with H265 format on Server 22.09. AES-146 <br>
Tag: Motion detection
Motion Detection Fails on HikVision DS-6716HUHI-K Encoder
Description The HikVision DS-6716HUHI-K encoder fails to record when set to motion detection recording schedule in exacqVision. Note: This device has been deprecated by the manufacturer. Product Steps to Reproduce Expected Results Motion is detected and video is recorded Actual Results Motion is not detected and video is not recorded Solution We have found that… Continue reading Motion Detection Fails on HikVision DS-6716HUHI-K Encoder
Samsung Motion Issues
Description Samsung cameras have experienced motion recording issues when running exacqVision Server version 22.09 or lower. Product Steps to Reproduce Expected Results Actual Results Solution It was determined this was a result of metadata timeouts and can be resolved by updating to exacqVision Server 22.12.3.0 or higher.
Holis camera is not recording motion
Description Holis cameras are not recording on Motion when connected to exacqVision server version 22.09 and earlier. Solution Update the exacqVision Server to version 22.12.0 or higher to fix the motion issue. <br>
Samsung QNP-6230x Motion not Working After Selecting a PTZ Preset
Description After selecting a PTZ preset motion appears to stop working in the camera’s web interface. If you edit the motion settings in the client, the motion will events will start to work in the camera again. Product Camera models: Firmware: Steps to Reproduce Have the camera setting on the home preset. Expected Results PTZ… Continue reading Samsung QNP-6230x Motion not Working After Selecting a PTZ Preset
Security Analytics & Intelligent Alerts Explained
Security Analytics & Intelligent Alerts Explained
Samsung Camera’s Motion settings are not showing up after updating to 21.12.2.0
Description Samsung motion settings disappear when last motion window is removed. Product ExacqVision Server 21.12.2.0 Steps to Reproduce Expected Results Motion Windows are removed and new motion windows can be created Actual Results Motion Windows are removed but Motion Window settings have disappeared Solution This has been resolved in exacqVision Server version 22.03 03/03/2022 v22.03.0… Continue reading Samsung Camera’s Motion settings are not showing up after updating to 21.12.2.0
Low Light Motion Setup
Problem In lower light conditions motion may be triggered constantly or not at all. This can be seen in the camera webpage as well where the last motion alarm is a start alarm followed by no stop. Solution To reduce the false triggers the following can be done. Reduce the sensitivity of the motion area.Draw… Continue reading Low Light Motion Setup
Troubleshooting Motion Not Supported
If you run in to an Exacq system where it says “Motion Not Supported” there are several camera manufacturers where you have to Enable Motion in the Web GUI of the device; as well as setting it in Exacq Client software. It will be listed under something like Analytics>Motion or Alarms or Motion.
Illustra 825 Pro Minidome Motion Detection Limitation
To enable motion detection on an Illustra 825 Pro Minidome in exacqVision, Stream 2 should always be set for H.264 video compression format with a resolution of 1920×1080 or less. The encoder chip in this camera generates motion notification only on an H.264 stream at that resolution or lower.