Removing MegaRAID Storage Manager(MSM)

Description MegaRAID Storage Manager (MSM) has been found to have some exposure to CVE-2021-44228, the Apache Log4j remote code execution vulnerability, see statement from Broadcom Log4j2 Exposure (CVE-2021-44228).   It is possible that MSM was installed on your exacqVision NVR even though a RAID controller card is not present. If that is the case MSM can… Continue reading Removing MegaRAID Storage Manager(MSM)

Replacing MegaRAID Storage Manager (MSM) With LSI Storage Authority (LSA) – Linux

Title Replacing MegaRAID Storage Manager (MSM) With LSI Storage Authority (LSA) – Linux Description MSM has been found to have some exposure to CVE-2021-44228, the Apache Log4j remote code execution vulnerability, see statement from Broadcom Log4j2 Exposure (CVE-2021-44228).   As a result you may be able to replace MSM with LSA on a Windows machine using… Continue reading Replacing MegaRAID Storage Manager (MSM) With LSI Storage Authority (LSA) – Linux

RtspServerPI may not be installed on Linux

Description RTSP server is no longer seen in the tree under Add IP camera after upgrade to 20.12. If the server version is rolled back to 20.09 it can be seen again. This does not seem to affect windows installs​ Tested Version 20.12.x Platform Linux Steps to reproduce install/update server Expected result rtspserverpi is installed… Continue reading RtspServerPI may not be installed on Linux

Enabling Core Dumps on Linux/Ubuntu with exacqVision Server

Beginning with exacqVision Server 9.8.x, enabling or disabling exacqVision core dumps may be performed as follows:To Enable: Open Terminal sudo touch /usr/local/exacq/server/enabledumps There is no need to restart the service for any reasonWithin 1 second, SysmgmtPI will log SYSMGMTPI: enabled core dumps If the server crashes, you may grab the dump file /usr/local/exacq/server/logs/core_dump.gz(Prior to 19.03.x, the location was /usr/local/exacq/server/blob/core_dump.gz)This… Continue reading Enabling Core Dumps on Linux/Ubuntu with exacqVision Server