LDAP connection requirements

Description:- In order to succeed in the remote client authentication via LDAP, We will need to make sure that we have the following three points. The way Kerberos tickets work is that we need all three points able to see and connect to each other, so we need to check these requirements before establishing the… Continue reading LDAP connection requirements

Enterprise Manager supports LDAP authentication with Azure Active Directory 

Azure Active Directory supports the LDAP interface when properly configured, and therefor LDAP can be used to sync the ExacqVision Enterprise Manager software with the Azure AD instance. Background Information: Lightweight Directory Access Protocol (LDAP) is an application protocol for working with various directory services. Directory services, such as Active Directory, store user and account… Continue reading Enterprise Manager supports LDAP authentication with Azure Active Directory 

LDAP Users Cannot Create User Views

Title LDAP Users Cannot Create User Views in Exacqvision Client   Description  Users logged in using LDAP cannot create user views in the exacqVision Client   Product  exacqVision Client   Steps to Reproduce  Login in as a exacqVision (not LDAP) userCreate a user view if there aren’t anyThere needs to exist at least one user view… Continue reading LDAP Users Cannot Create User Views

AES Encryption Methods Supported For LDAP Connection

AES-128 and AES-256 encryption support for LDAP communication was added with the release of exacqVision Server 21.12.3. Versions older than that must use RC4 encryption. To determine if you are using the AES encryption or not. Check the logs from Exacq server for the StreamPi plugin, and if you are using the AES encryption and… Continue reading AES Encryption Methods Supported For LDAP Connection

Mac Clients having issues connecting to LDAP

Encountered on : Ventura 13.5 and above We need to make sure that the client machine is Joined to the Domain via the GUI method using the instruction in the following link from Apple. https://support.apple.com/guide/directory-utility/configure-domain-access-diru11f4f748/mac Encountered on : BIG SUR 11.4Behavior: MAC Clients are not able to connect to the Domain Using LDAP only. We… Continue reading Mac Clients having issues connecting to LDAP

LDAP user First time logging in from client to ESM results in Error

Description From the client’s “Synchronize with ESM” page, using an LDAP username and password results in ‘Check your URL’ error. This happens even though the LDAP domain and group associations (with ESM access) is correctly configured on ESM. <br> Tested version 4.8.2 <br> Platform All <br> Steps to reproduce Create a domain and associations on… Continue reading LDAP user First time logging in from client to ESM results in Error

Automatic creation of Service Principal Name (SPN)

Starting with exacqVision 7.2, the server has the ability to automatically create its own service principal name (SPN). A valid SPN is required in order to enable single-sign-on. To enable this feature: Check the box next to “Permission to create SPN” on the LDAP/Active Directory settings page.Verify with your domain admin that the bind account… Continue reading Automatic creation of Service Principal Name (SPN)