Description When connecting exacqVision Server to Entrapass versions 8.62 & 8.70 or updating Entrapass to these versions, it will stop showing the inputs in exacqVision. Product exacqVision Server any version with Kantech Entrapass ver 8.62 & ver 8.70. Steps to Reproduce Expected Results All Kantech inputs are displayed. Actual Results Solution The Kantech team has… Continue reading Kantech – Entrapass ver 8.70 & 8.62 stops showing the outputs and inputs in exacqVision
Tag: Kantech Entrapass
Can’t Set an Email Profile When Kantech Software is Connected to The Exacq Server
Description When having Kantech Board connected to the Exacq Server, Client Software keeps refreshing the configs and that prevents the Exacq client from creating an Email notifications profile. affected version is 23.03 or lower Solution Updating ExacqVision Server and Client to version 24.03 or above. Updating the Kantech Entrapass to version 8.80 or above.