Description The following is a list of default port numbers used by exacqVision software. NOTE: Many ports listed below may only used with certain configurations or by optional services and integrations. Products Port List PortDescription25Simple Mail Transfer Protocol (SMTP)80exacqVision Web Server/exacqVision Enterprise Manager (HTTP)How to change Web Service portsHow to change EM web ports389LDAP (Lightweight… Continue reading exacqVision Default Ports
Tag: iSCSI Storage
Video Not Recording to iSCSI with Status “Recording Not Possible”
Description Video is not recording to customers iSCSI targets after a reboot. Drive was reporting a status of “Recording Not Possible” on exacqVision Server 21.03.10. Servers running exacqVision Server version 20.06 or older were showing a status of healthy, but were not recording. Identification Use the following to properly identify the issue before applying the… Continue reading Video Not Recording to iSCSI with Status “Recording Not Possible”
Enabling iSCSI Support on exacqVision Systems with Windows Embedded
Early versions of exacqVision systems with the Windows Embedded operating system did not have support for iSCSI. These systems were manufactured in in January and early February 2014. To determine whether a system supports iSCSI, complete the following steps: Open the Start menu.Right-click Computer.Select Manage from the pop-up menu.Double-click Services and Applications.Double-click Services.If Microsoft iSCSI… Continue reading Enabling iSCSI Support on exacqVision Systems with Windows Embedded
Set iSCSI Storage to Start Before ExacqVision Server in Windows
If you are recording video to an iSCSI target in Windows, it is important to ensure the iSCSI device is available in the operating system before the ExacqVision Server starts. Please follow the instructions from the Microsoft iSCSI Software Initiator Version 2.x Users Guide: Note: The following information was written and published by Microsoft Corporation,… Continue reading Set iSCSI Storage to Start Before ExacqVision Server in Windows