Configuring IP Addresses on a Cloudvue Gateway

Description  This article describes how to set IP addresses as either static or DHCP for a Cloudvue Gateways onboard NICs. Product  Prerequisites Solutions NOTE: Network Settings can only be viewed, not changed from cloudvue.com Local Cloudvue Command Line In this example both NICs em2 (LAN) and em1 (Cameras) are being set to a static IP… Continue reading Configuring IP Addresses on a Cloudvue Gateway

How multiple adapters on the same network are expected to behave

Summary If you configure a Windows-based computer that has more than one network adapter on the same physical network and protocol subnet, you may experience unexpected results. This article describes the expected behavior of this kind of nonstandard configuration.  More Information Consider the following scenario: In this scenario, you may expect the two adapters on… Continue reading How multiple adapters on the same network are expected to behave

Why do I see the 127.0.0.1 IP address in my Add Systems list?

Modern computer networks require each device on the network to have a unique IP address. These addresses are used so that computers know how to communicate with each other and so that network equipment knows where to route the traffic crossing its path. When using the ExacqVision Desktop Client application from a client workstation to… Continue reading Why do I see the 127.0.0.1 IP address in my Add Systems list?