Connecting an Illustra Camera to Two Servers Simultaneously

Description This article outlines the available methods for connecting a single Illustra camera to two servers at the same time. This is useful for environments where two recording or monitoring systems need simultaneous access to the same camera feed. Product Illustra IP Cameras exacqVision Server Solution Option 1 — Recommended Method (Official) Option 2 —… Continue reading Connecting an Illustra Camera to Two Servers Simultaneously

Illustra Camera RTSP strings

Introduction This article outlines the RTSP Strings for Illustra cameras Illustra Fisheye Gen1 Primary Stream:rtsp://[username]:[password]@[CameraIP]:7779/primarystreamSecondary Stream:rtsp://[username]:[password]@[CameraIP]:7781/secondarystreamPrimary Video & Audio:rtsp://[username]:[password]@[CameraIP]:7778/primarystreamSecondary Video & Audio:rtsp://[username]:[password]@[CameraIP]:7780/secondarystreamAudio Stream:rtsp://[username]:[password]@[CameraIP]:7777/audio Illustra Fisheye Gen2 Stream1 Video:rtsp://[username]:[password]@[CameraIP]:554/videoStreamId=1Stream1 Audio:rtsp://[username]:[password]@[CameraIP]:554/audioStreamId=1Stream1 Video & Audio:rtsp://[username]:[password]@[CameraIP]:554/videoStreamId=1&audioStreamId=1ONVIF:rtsp://[username]:[password]@[CameraIPaddress]:554/onvif/videoStreamId=1 Illustra Fisheye Gen4 Stream1 Video:rtsp://[username]:[password]@[CameraIP]:554/videoStreamId=1Steam2 Video:rtsp://[username]:[password]@[CameraIP]:554/videoStreamId=2Steam3 Video:rtsp://[username]:[password]@[CameraIP]:554/videoStreamId=3 Illustra Flex Gen2 Stream1 Video:rtsp://[username]:[password]@[CameraIP]:554/videoStreamId=1Stream1 Audio:rtsp://[username]:[password]@[CameraIP]:554/audioStreamId=1Stream1 Video & Audio:rtsp://[username]:[password]@[CameraIP]:554/videoStreamId=1&audioStreamId=1ONVIF:rtsp://[username]:[password]@[CameraIPaddress]:554/onvif/videoStreamId=1 Illustra Pro Gen2 Stream1 Video:rtsp://[username]:[password]@[CameraIP]:554/videoStreamId=1Steam2 Video:rtsp://[username]:[password]@[CameraIP]:554/videoStreamId=2ONVIF:rtsp://[username]:[password]@[CameraIPaddress]:554/onvif/videoStreamId=1 Illustra… Continue reading Illustra Camera RTSP strings

Add IP Cameras – Quick Add

Description The Quick Add tab, found on the Add IP Cameras page of the exacqVision Client is a recently added feature. Introduced in version 24.03, this feature accelerates the configuration and addition of supported camera models to your exacqVision system. <br> Products Quick add requires both exacqVision Server and exacqVision Client versions 24.03 or higher.… Continue reading Add IP Cameras – Quick Add

Using the Illustra License Registration Tool

Overview Users entitled to free IP camera licensing from eligible Illustra cameras may easily claim a new license key for their exacqVision system online, without the need to contact Orders. NOTE: It is best practice to declare your eligible cameras and apply the generated license as a first step during NVR setup to prevent those… Continue reading Using the Illustra License Registration Tool

Illustra Multisensor Backwards Compatibility

Background Over many years the number of Illustra camera related plugins had grown. An engineering effort was aimed at consolidating these to make selection of the appropriate plugin easier for users. exacqVision Server 24.03 represents a configuration shift which could affect users that attempt to downgrade the server application to versions earlier than 24.03. This… Continue reading Illustra Multisensor Backwards Compatibility

Edge Server Application Stops Shortly After Starting on Illustra Cameras

Description Users setting up the ExacqVision Edge or Edge+ application on Illustra cameras may see the application running and connect to it only to find it stops running shortly thereafter. This is likely due to changing the default ‘Enable Event Record’ setting on the camera. <br> Product Cameras: Edge Server <br> Steps to Reproduce <br>… Continue reading Edge Server Application Stops Shortly After Starting on Illustra Cameras

Failure to Receive Events from Illustra Pro Gen4 Multisensor

Description Users fail to receive alerts and/or ExacqVision actions configured through Event Linking or Event Monitoring fail to occur when using an Illustra Pro Gen4 Multisensor camera as the source. <br> Product <br> Steps to Reproduce None. This issue exists in firmware prior to Illustra.SS017.06.05.00.0008 <br> Expected Results Analytic events, including those caused by motion… Continue reading Failure to Receive Events from Illustra Pro Gen4 Multisensor

Exacq Scenario Series – Illustra IQ Perimeter Object Classification to Change ExacqVision Views

The Scenario Series of videos addresses setup configurations for specific use cases. In this video our scenario is that of a user that wants to use Event Monitoring to bring attention to an ExacqVision operator when a perimeter area is crossed. This could be used to monitor property and fence lines. We walk through setting… Continue reading Exacq Scenario Series – Illustra IQ Perimeter Object Classification to Change ExacqVision Views