The expansion of the market for security cameras equipped with AI features has led to a substantial increase in the volume of metadata transmitted from these devices. While this growth opens up valuable opportunities for enhancing the usability of stored video—such as enabling searches for specific objects (like people and vehicles) and their attributes (such… Continue reading Deciding to Store AI Bounding Boxes
Tag: Hard Disk
False Drive Offline status on some Q-series models
Description Some drives may show an “offline” status on the hardware tab in ExacqVision Client when Server Version 23.03.1.0 is installed on Q-series models, though data can be read from and written to the drive.Note: This issue manifests itself cosmetically by appearing as if the drive is offline but has no bearing on functionality for… Continue reading False Drive Offline status on some Q-series models
2021-02 – Hard Drive Issues Training
Hard Drive Issues Troubleshooting
Server May Indicate False HD Temperature Alarms on Systems with LSI RAID
Symptom Client displays temperature alarms on hard drives. These may indicate temperatures near 1° C, or between ~20000-30000° C. <br> Problem This behavior was seen from the following Western Digital HD models when connected to LSI storage controllers. WD4002FYYZWD8002FRYZWD8003FRYZWD6002FRYZWD80PUZXWD101KRYZWD121KRYZ <br> Solution Update the ExacqVision Server version to 9.3.9 or higher, also back-patched into 9.2 RC. <br>
Supporting HDD SMART Data on Third-party Hardware
When installing ExacqVision Server software, including its System Management plugin on third-party hardware, you should aim to use a RAID controller used in Exacq manufactured systems, which include: If a different controller (or no drive controller) is used, the behavior of the system will vary. SMART data from a drive controller is handled by Smartmontools.… Continue reading Supporting HDD SMART Data on Third-party Hardware