Hanwha PNM-C32083RVQ Connection to Server and Motion Stops Working

Description  Hanwha will not allow motion to work properly with Exacq Server 24.09.4.0 as long as the camera is on fw 23.01.04-20240417-R929 due to a NTP issue found. Another issue reported is the connection status will throw errors to indicate it is not connected properly.NOTE:FW 23.01.01 obtained from Hanwha (which will be the official release… Continue reading Hanwha PNM-C32083RVQ Connection to Server and Motion Stops Working

The Samsung Plug-in May Stop all Processing Because of Unexpected Data Received from Newer Hanwha Cameras

When attempting to add a camera with the Samsung plug-in (SamsungPI), newer models of Hanwha cameras with newer firmware versions have been observed to cause the Samsung plug-in to stall. This event will prevent the processing of the remaining (already-configured) Samsung and Hanwha cameras. The camera will sit on “connecting” and no error message is displayed.