Product Exacq Server 26.0.3.0 Windows and Linux. Steps to Reproduce Add camera to client.Navigate to Digital PTZ/Fisheye tab under Add IP Cameras.Select drop down menu for the Fisheye dewarp.Editing from Generic Ceiling, Ground, and Wall adds a giant black bubble on the live view. Editing the Generic options of X,Y, and R does not remove… Continue reading Axis Dewarper Not showing for the F9114 and F9114R-Mk II
Tag: Fisheye
MAC OS Axis Dewarper
Description: Mac OS Clients do not show Axis Dewarper options in the camera setting page. Product: ExacqClient 26.0.2.0 Reason: Axis provides their own proprietary dewarping module, and currently they have not released a Mac ARM–compatible version. Because of that limitation on the Axis side, the only available option on macOS ARM devices is to use… Continue reading MAC OS Axis Dewarper