Associations Not Allowed to be saved as Momentary or Sustained Option

Description  When setting up a new association there is no options in the drop down menu for Momentary or Sustained when setting up Associations. Display only is seen as the only option available. This was exhibited on Server/ Client software starting on 23.09 through 24.12.7. Product  Steps to Reproduce  Upon update from 23.06 Server/Client to… Continue reading Associations Not Allowed to be saved as Momentary or Sustained Option

Added Axis Dewarping on Axis M Series Cameras

Description  Reports stating the Axis dewarper sometimes shows up in our software and other times doesn’t for different models. 2nd issue stated that the generic dewarper is “elongated” or distorted when zooming in via digital PTZ and panning or tilting the camera. Product  Steps to Reproduce  tried different formats H.264/H.265tried different resolutions–>no changetried Ceiling/WallTried Digital… Continue reading Added Axis Dewarping on Axis M Series Cameras