Tag: Events
Failure to Receive Events from Illustra Pro Gen4 Multisensor
Description Users fail to receive alerts and/or ExacqVision actions configured through Event Linking or Event Monitoring fail to occur when using an Illustra Pro Gen4 Multisensor camera as the source. <br> Product <br> Steps to Reproduce None. This issue exists in firmware prior to Illustra.SS017.06.05.00.0008 <br> Expected Results Analytic events, including those caused by motion… Continue reading Failure to Receive Events from Illustra Pro Gen4 Multisensor
Event Linking
Event Linking gives you the power to create automated actions based on your selected events. Sending email notifications when motion is detected, activate an alarm output when an input trigger is detected, automatically export a video clip when a button connected to an input is pressed, turn a PTZ camera to a preset point if… Continue reading Event Linking
Configuring Views that Change Based on Events
Introduction A useful feature of exacqVision Client is to automatically switch to a view that highlights an event in progress. This can be configured two slightly different ways in exacqVision Client: <br> Configuration Steps Each of these methods are explained in the following sections. Configuring Event Monitoring using a Default View and the Event Monitoring… Continue reading Configuring Views that Change Based on Events
Configure Event Linking to Include Video in Notifications Triggered by Non-Video Events
Description Starting with exacqVision 5.10, you can configure email notifications to include a video clip or still image from one or more cameras even if the event does not directly involve video (that is, if the event is not video motion, video loss, IP camera connection, or analytics) using Source Groups to associate video to… Continue reading Configure Event Linking to Include Video in Notifications Triggered by Non-Video Events
What is the limit on the number of Event Linking entries I can create?
There is no programmed limit to the number of Event Linking entries you can create. However, if you set up more than 50 Event Linking entries, it is a good idea to deselect the Log checkboxes displayed to the left of the event listing. The log file can grow to an unstable size if you… Continue reading What is the limit on the number of Event Linking entries I can create?