Description If you enable Restricted View on Cameras Setting page of our client this can cause certain integrations to not show the live streams. For Example an integration such as CCure9000 will not show the streams on the Ccure interface seen below. Product Steps to Reproduce In the Exacq Client if you enable Restricted View… Continue reading Restricted View evAPI and Integrations
Tag: evAPI
Axis P3247-LVE “Axis Object Analytics” not passing through the Exacq Mobile 3 app Analytic Rules
Description Axis P3247-LVE “Axis Object Analytics” not passing through the Exacq Mobile 3 app Analytic Rules. If seen please see AES-609. Escalate the case to be added to ticket. Product Steps to Reproduce Set up the camera to allow analytics. Note we do not support line cross for axis cameras. Expected Results We should be… Continue reading Axis P3247-LVE “Axis Object Analytics” not passing through the Exacq Mobile 3 app Analytic Rules
Password Strengthening and Augmented Authentication Integration with S2
If this setting is enabled then it is possible with certain version of Server software, an API issue could occur. Specifically with the OVID plugin when integrating with S2. Product TESTED Version:Client Version: “22.12.2.0”Server Version: “22.12.5.0”evOVID plugin version 1.1.12.123380 Steps to Reproduce If the Password Strengthening and Augmented Authentication is enabled then OVID plugin will… Continue reading Password Strengthening and Augmented Authentication Integration with S2
exacqVision SDK / API and OEM Solution Partner Requests
Title exacqVision SDK / API and OEM Partner Solutions Summary exacqVision SDK & OEM Solutions, we are part of the Connected Partner Program, so all request must first register via the Connected Partner Portal to be considered. Description Exacq Technologies provides integration tools that enable dealers and development partners to rapidly integrate external devices and… Continue reading exacqVision SDK / API and OEM Solution Partner Requests
How to: Using EVAPI_Discover to Detect the Connectiodn to an exacqVision Server
Overview The EVAPI_Discover function is used to test the connection between evAPI and an exacqVision server. When EVAPI_Discover is called, it initiates a Discover request to be sent to an exacqVision server. If the Discover request is received by the server, it sends a Discover response indicating the server was found. <br> Usage It is… Continue reading How to: Using EVAPI_Discover to Detect the Connectiodn to an exacqVision Server
How to: Executing and debugging C# applications with evAPI and Visual Studio 2005 or newer
C# or other managed applications created with Visual Studio 2005 or newer cause a System.AccessViolationException in the EVAPI_CreateWindow function on Windows Vista and Windows 7. To avoid this while debugging within Visual Studio and during application execution, complete the following steps. After the project has loaded, select the project properties under the Project item on… Continue reading How to: Executing and debugging C# applications with evAPI and Visual Studio 2005 or newer