Description The ePlayer shortcut is missing from the menu. The player is still there and can be launched from the command line <br> Version Introduced 7.9.20 <br> Platform Linux <br> Steps to reproduce Install client deb <br> Expected result ePlayer shortcut under Exacq menu <br> Actual result Only client shortcut under Exacq manu <br> Work… Continue reading Missing ePlayer shortcut on Linux