Description exacqVision Edge is a complete video management system (VMS) software solution that runs directly on an IP camera and stores video to an microSD/SD card inserted in the camera. Supported Devices Use the filters on the exacqVision IP Camera Integration database to search for devices that support exacqVision Edge. Installers Download the appropriate installer for… Continue reading Setup and Licensing exacqVision Edge/Edge+
Tag: Edge
Edge Server Application Stops Shortly After Starting on Illustra Cameras
Description Users setting up the ExacqVision Edge or Edge+ application on Illustra cameras may see the application running and connect to it only to find it stops running shortly thereafter. This is likely due to changing the default ‘Enable Event Record’ setting on the camera. <br> Product Cameras: Edge Server <br> Steps to Reproduce <br>… Continue reading Edge Server Application Stops Shortly After Starting on Illustra Cameras
Updating Camera Firmware When Using ExacqVision Edge
The ExacqVision Edge and Edge+ software runs a single-camera ExacqVision server instance directly on supported camera models. To perform camera firmware updates, we recommend the following steps. <br>
Edge Plus Archive Options
exacqVision Edge Plus Archiving currently supports SMB archiving targets. Edge Plus does not currently support Cloud Drive or Amazon S3 archiving. <br>
Illustra IPS02-P24-OI04 Fails to Load exacqVision Edge
Description The exacqVision Edge software will not load successfully on the camera. A factory default of the camera will be required to undo the software installation attempt and recover normal operation of the camera. Product Steps to Reproduce Expected Results The exacqVision Edge software would load properly and be accessible to license from an exacqVision… Continue reading Illustra IPS02-P24-OI04 Fails to Load exacqVision Edge
What Files Are Stored To The SD Card In Axis Edge Installs
*** INTERNAL *** Here is a listing of all the files that sit on the SD card in an Axis Edge installation. The size of all installed files with no recording is around 25MB Disk space listing of SD card (cmd: du -h /var/spool/storage/SD_DISK): 64.0k ./exacq/logs 64.0k ./exacq/audit 32.0k ./exacq/blob 18.9M … Continue reading What Files Are Stored To The SD Card In Axis Edge Installs