False Drive Offline status on some Q-series models

Description  Some drives may show an “offline” status on the hardware tab in ExacqVision Client when Server Version 23.03.1.0 is installed on Q-series models, though data can be read from and written to the drive.Note: This issue manifests itself cosmetically by appearing as if the drive is offline but has no bearing on functionality for… Continue reading False Drive Offline status on some Q-series models

Replacing a Drive in an LSI 3ware RAID Array

To install a replacement drive in an exacqVision system with an LSI 3ware RAID array, complete the following steps.<br> NOTE: This procedure requires a Phillips-head screwdriver and approximately 20 minutes to complete.<br> If applicable, close the exacqVision Client software, log out of the operating system user account, and log in as an administrator. To log out… Continue reading Replacing a Drive in an LSI 3ware RAID Array

SMART attributes now available for drives connected to LSI storage controllers on Windows using exacqVision 7.6

Affected Platforms exacqVision 7.6 Description LSI has added support for SMART attributes in the storcli utility in version 1.12. Users can now monitor all SMART attributes for drives connected to LSI controller on Windows using exacqVision server 7.6.0 or higher. Users using a version of storcli without SMART support will continue to see only the… Continue reading SMART attributes now available for drives connected to LSI storage controllers on Windows using exacqVision 7.6

Windows-based ExacqVision Systems Must Record Directly to Fixed Drives

The Windows version of ExacqVision Server must record directly to drives that Windows identifies as fixed drives, such as iSCSI drives. Network-attached storage (NAS), or mapped drives, cannot be used for direct recording because the ExacqVision system cannot detect whether the drives are being used for other purposes. Such conflicts can cause recording issues on… Continue reading Windows-based ExacqVision Systems Must Record Directly to Fixed Drives