Q87-based Windows exacqVision System Driver_Power_State_Failure BSOD

If a Q87-based Windows exacqVision unit experiences a BSOD with the reference Driver_Power_State_Failure, you should update the USB 3.0 drivers to at least 3.0.5.69. This will prevent the BSOD from occurring based on USB issues with the motherboard.To install the driver, complete the following steps: Download the file from Intel.Right-click the .zip file and select Extract All.When… Continue reading Q87-based Windows exacqVision System Driver_Power_State_Failure BSOD