False Drive Offline status on some Q-series models

Description  Some drives may show an “offline” status on the hardware tab in ExacqVision Client when Server Version 23.03.1.0 is installed on Q-series models, though data can be read from and written to the drive.Note: This issue manifests itself cosmetically by appearing as if the drive is offline but has no bearing on functionality for… Continue reading False Drive Offline status on some Q-series models

How to Determine if a Drive is Read-Only

In Linux systems a filesystem error may cause a storage volume to be re-mounted by the operating system as Read-Only. This could be evident on the Storage page under the Drives tab when the volume status changes to ‘Write Error’ or when you attempt to search for video and find the system does not appear… Continue reading How to Determine if a Drive is Read-Only

ExacqVision A-Series 4U Drive Replacement Guide

NOTE: This article assumes that you already know which drive number must be replaced, and that you have a replacement drive ready to install in the system.NOTE: The photos in this article illustrate the replacement of Drive 3.To replace a hard drive in an exacqVision A-Series 4U system manufactured on or after 07/30/2015, complete the following steps:… Continue reading ExacqVision A-Series 4U Drive Replacement Guide